AXIS#.BODE.VFLIMIT

Description

When AXIS#.BODE.MODE is set to 5, the firmware monitors the drive feedback velocity AXIS#.VL.FB. When AXIS#.VL.FB goes above AXIS#.BODE.VFTHRESH, an internal counter records the length of time AXIS#.VL.FB was above AXIS#.BODE.VFTHRESH. If the internal counter reaches AXIS#.BODE.VFLIMIT, Fault F6003 – Instability during Autotune will be generated.

The smaller AXIS#.BODE.VFLIMIT, the quicker Fault F6003 will be generated when AXIS#.VL.FB exceeds AXIS#.BODE.VFTHRESH.

Example

Set AXIS1.BODE.VFTHRESH to 10 RPM:

--> AXIS1.BODE.VFTHRESH 10

Set AXIS1.BODE.VFLIMIT to 0.500 seconds:

--> AXIS1.BODE.VFLIMIT 0.5

Set AXIS1.BODE.MODE to 5 to enable stability detection:

--> AXIS1.BODE.MODE 5

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Description

Sets the current fault duration limit in seconds for the AXIS#.BODE.MODE 5 stability test

Units s

Range

0 to 60.000

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

No

 

Variants Supported

All variants are supported

Related Topics

Tuning Fundamentals | Understanding a Bode Plot